Click this button to collect current information about the set of waveform files that are saved in the test set's default ARB waveform directory, D:\NVARB. The waveform file names will then appear in the dropdown list of values for the “Waveform” parameter in the source setup table. Sequence Studio must be connected to the test set for this information to be collected.